12/11/2008 7:56 AM | |
Posts: 37 Rating: (0) |
Greetings. Can anyone advise if the attached OLM Topology is valid? It is one half of a redundant pair but i have only shown one network for clarity. Thanks in advance. AttachmentOLM Topology.pdf (223 Downloads) |
12/11/2008 3:57 PM | |
Posts: 5822 Rating: (412)
|
Dear gfair, I hope you are aware of the fact that single fiber optical rings are not release for the OLM G or P series anymore. If you want to have redundancy you need to use either OLM P12 or G12 and you use a redundant ring with two fibers for each interconnection between OLM’s. J_Bell |
12/12/2008 3:04 AM | |
Posts: 37 Rating: (0) |
Thanks J_Bell I wasn't sure if single fibre was allowed. I had read the Manual for OLM but couldn't find what I was looking for. I have a new Topology which i think will meet our requirements. AttachmentStage C OLM Topology 2.pdf (191 Downloads) |
Last edited by: gfair at: 12/12/2008 3:43 AM |
|
Follow us on