10/26/2017 11:10 AM | |
Joined: 6/17/2014 Last visit: 5/21/2023 Posts: 4 Rating:
|
Hello, I installed step7 V5.5SP3 Inside a virtual machine VMWARE WORKSATION V10.0(Host Windows 7, Guest Windows XP SP3). Impossible to work fine the ISO simatic protocol with step7 to card CP343-1 343-1EX21-0XE0. Step7 shows me available partners but if i try to see "Status Module" with the function "Target System, it doesn't work. On the ohter hand, TCP/IP works properly. In my physical machine(Windows 7), Step7 with ISO and TCP/IP works fine All firewalls are unchecked. ISO SIMATIC PROTOCOL supported Inside VM machine? You will find snapshots from ma virtual machine. Thank you for your help guys.
AttachmentStep7VmwareISOProblem.zip (95 Downloads) |
10/26/2017 1:41 PM | |
Joined: 7/9/2015 Last visit: 3/25/2025 Posts: 4207 Rating:
|
Hi, first check information of you error code in the PDF in the following LINK. Here you will find information on the remedy https://support.industry.siemens.com/cs/de/en/view/770453 I recommend to update to V5.5 SP4. With this version you can use VMware Workstation 10.0 - with SP3 I am not really sure if everything will work - I can´t find any releases for VMWare with V5.5 SP3. Regards, Towome |
|
|
Follow us on