12/4/2012 2:56 PM | |
Posts: 14 Rating:
|
Hi Guys, I have configured an ABB RTU560 as IEC 61850 server and SICAM PAS ver6 (demo version) as 61850 client. 61850 interface in SICAM PAS runtime ver6 was established without any problem and points configured in RTU were updated in the client. I carried out some tests on ABB points and checked with value viewer successfully. But same test failed in SICAM PAS ver7.01 (demo version) My ABB.iid file (exported from RTUtil560 v10.5.2.0) can’t be imported in Sicam v7.01. It returns an error message (attached jpg file) on importing stage, stating that "Both columns Main AP and Main IP address must either be filled or be empty!". (while it was imported in Sicam ver6 without such error). Since *.iid file exported from RTUtil doesn’t contain IP address, so to solve this problem I imported the iid file into CCT600 software, and using CCT, I created *.icd file (assigned with proper IP address) and tried to import it into SICAM PAS but it doesn’t accept .icd file extension. Accepted extensions are .scd, .iid, .cid. So I imported ABB.icd file into digsi and exported *.scd file from digsi then I imported .scd file to SICAM PAS. It was imported without error but in runtime, the 61850 interface failed and ABB RTU wasn’t connected. Again same SCD can be imported into SICAM PAS v6 and connect to the RTU without any problem. Attached is the scd file imported in SICAM v6 and v7 and exported mapping from the device, in v6 and v7. Please advice what I should do to fix this issue... Thanks Artin AttachmentABB RTU560 To SICAM PAS.zip (393 Downloads) |
7/31/2014 3:08 PM | |
Joined: 9/1/2005 Last visit: 1/28/2025 Posts: 4114 Rating:
|
|
My Forum is the place to personalize your profile, |
|
Follow us on