3/15/2022 7:23 AM | |
Joined: 1/18/2022 Last visit: 10/4/2022 Posts: 2 Rating:
|
I migrated panel from ProTool to WinCC and then to TIA Portal. But I can't migrate the PLC Step 7 project. There is an error: "Option package(s) PROTOOL missing in STEP 7 version V5.6 + SP1." It is impossible to install ProTool together with TIA Portal in Windows 10. I think the HMI project is integrated with Step 7 PLC project, and for that reason, I can't migrate it in TIA. After removing the panel and compiling the project, the problem persists. Is there any solution for that? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/15/2022 12:59:01New subject after splitting |
|
Follow us on