1/15/2016 2:40 AM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating:
|
Hello dear colleagues, I will describe my application and problem as best as i can: In our machine we have a profinet network in which we have IWLAN comunication with several ET200S, we choose to use IWLAN because ET200S are moving arround in the machine, each ET200S is mountend in a sort of cart, we have 20 carts in the line in a kind of carrousel arrange (please check Fig #1 in attached PDF). All of the carts moves and turn arround the machine as showed by the arrows in Fig #1, the speed at which they move is about 12.3 Meters per minute, the length of the machine from side to side is about 45 meters, and the width is about 10 meters. Inside of the machine carrousel we have 3 access points Scalance (6GK5788-1GD00-0AA0), this access points are located in the positions AP1, AP2 and AP3; inside each cart cabinet we have 1 client Scalance (6GK5747-1AA30-6AA0) which we use as gateway to link the corresponding ET200S with the acces points, and finally the acces points are linked to the Profinet IO network; the network topology is shown in Fig #2 of the attached PDF. The problem that we have is that under this conditions, we loss comunication with 1 or more clients in a ramdom way, the comunication loss is normally instantanius (it does last no more than 4 seconds), we think that time, is the time that the client needs to switch from a acces point to another. As mentioned before the comunication loss happen in random way, there is no repetition pattern, all of the clients may loss comunication in different zones of the machine, and under different circumstances; even when the machine is not moving. We have reviewed the hardware conditions, by checking that all connectors (in the acces points, clients and ET200S) are clean, tight and in good shape, we also have repalced some of the ethernet cables used to link the ET200S with the clients, but so far this did not make any difference. Based on this description would you please suggest were to start so we may avoid to losse comunication with our ET200S, this fault may appear very offten, maybe 2 or 3 events per hour. Thanks all of you for your kid help. Regards
AttachmentReporte Acces Engs.pdf (273 Downloads) |
Keep working! |
|
1/15/2016 12:14 PM | |
Posts: 18 Rating:
|
The data records of one of the clients are attached here. |
1/19/2016 8:11 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating:
|
Hello Sicolinx, thanks a lot for sharing your knowledge and experience, at my machinne we are working at 5GHz, and we are working on 802.11g, so for shure i will change my system to work at 2.4GHz, and test it. Also i have upgraded the firmware of the acces points as well as the clients to the latest avaiable version, after this i let the system work for a couple of days, i monitored it, but the problem is still there. Then i have downloaded the event log files from all acces points as well as for some clients, by monitoring the online status of some of the clients i could not found any error or event report generated in the event log when the comunication is lost, but if someone would like to take a look to them, i'm attaching Several TXT files with them. Local Siemens product support (Mexico) suggested to change the network speed from 54MBbps to an slower rate (maybe 11MBbps) which sounds reasonable, and also change the update rate of the ET200S from 16 to 32 ms (in HW configuration) which from my point of view may not help, what do you think about this suggestions? Thanks all of you for your hel, have a grat day AttachmentWiFi_logs.zip (224 Downloads) |
Keep working! |
|
Follow us on