7/28/2011 2:10 PM | |
Joined: 8/31/2010 Last visit: 1/31/2023 Posts: 1498 Rating:
|
Hi. i need the libraries and sample projectfor Step 7 v11. Kindly provide the v11 project and libraries for PID. Splitted from TIPS for PID (FB PID_Compact). |
Last edited by: O_Moderator at: 8/15/2011 8:07 AMQuote added Last edited by: O_Moderator at: 7/28/2011 2:15 PMnew subject after splitting Like it? Rate it! |
|
7/29/2011 1:11 PM | |
Joined: 8/31/2010 Last visit: 1/31/2023 Posts: 1498 Rating:
|
The below mentioned is from your tip (TIPS for PID (FB PID_Compact)). 4 PID goes to inative mode (e.g. after power on). Two possible causes: 4a PV or SP are invalid or out of range: Take a look at the FAQ:"How can you prevent your S7-1200 PIDCompactcontroller from going inactive in the case of a PLC power cycle and invalid process values?" (http://support.automation.siemens.com/WW/view/en/46163827) 4b Monitoring time fault: How can you restart a PID controller stopped by sample time failure or disable the sample time monitoring? See FAQ: http://support.automation.siemens.com/WW/view/en/42321471 I need these two libraries for v11. Though I have not checked whether the v10 library will work in v11 without any issue. If it will work without any considerations then it's not an issue, otherwise these two libraries are required very urgently Thank You |
Like it? Rate it! |
|
8/3/2011 12:47 PM | |
Joined: 9/23/2005 Last visit: 1/31/2023 Posts: 4177 Rating:
|
Hi, in the original post (Tips for PID (PID_Compact) - /tf/WW/en/Posts/33957#top), I place a block to reset the inactive mode automatically. Despite it was made for 10.5, I belive that should be adaptede to V11 easly. |
Denilson Pegaia |
|
Follow us on