9/22/2021 9:28 AM | |
Joined: 12/17/2020 Last visit: 11/23/2022 Posts: 10 Rating:
|
Hello! This document says that the "MC_MoveLinearAbsolute" function performs a circular motion. And then how to perform a linear movement? |
Last edited by: Jen_Moderator at: 09/22/2021 13:17:17Optimized link. |
|
9/22/2021 10:03 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Shlykov, this must be an error in the documentation. Read the complete description, it is definitive linear path motion. in the german manual there is the correct text. MC_MoveLinearAbsolute: Position kinematics with linear path motion V5 hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
9/22/2021 10:36 AM | |
Joined: 12/17/2020 Last visit: 11/23/2022 Posts: 10 Rating:
|
Thanks for the explanation, mops04! I suspected that this was a mistake. I would like to see corrections made to the documentation, because this error passes from version to version. The same error occurs in the function description for TIAP 15 and TIAP 17. |
Follow us on