Industry Online Support
Technical Forum
6/5/2013 10:41 AM | |
Posts: 42 Rating:
|
hi the question is, when the project is loaded to the panel, it is necessary that the buttons are illuminated when the choice comes down to it. Thanks
|
6/5/2013 4:53 PM | |
Posts: 3037 Rating:
|
Hello, Do you want that after the project download the change to the old project should change the color? Tweety |
6/6/2013 8:17 AM | |
Posts: 42 Rating:
|
No panel can be for example buttons. And so. when I'm on the panel, flick up and down arrow keys are illuminated the element which I choose |
7/26/2016 8:06 AM | |
Posts: 106 Rating:
|
Hi did you tried button properties - Design - Focus try to set Width to the 5 or more and choose the color you want. |
Follow us on