6/14/2012 9:29 AM | |
Posts: 2 Rating:
|
Hi! I have a 10 KTP 400 in my application. All KTP 400 has the same application inside, only profinet address is different. This configuration is working about one year. So one morning 2/10 KTP 400 has a sligltly moved touch screen - cca1.5 cm from a button. I send a question to customer support and this is answer - quote: Please make following: - install TIA V11 SP2 UPD3 then make - OS Update with Reset to factory settings. - Colibrate again. But ist very IMPORTANT you should (Tap the screen to register saved data) Touch the cross in the screen center once again using the touch pen or your finger to confirm your entries, NOT waiting 30sek. Servicepack 2 für WinCC V11 http://support.automation.siemens.com/WW/view/en/56897511?Datakey=47069298 Updates for STEP 7 V11 SP2 and WinCC V11 SP2 http://support.automation.siemens.com/WW/view/en/58112582?Datakey=47069298 How do you do an operating system update (OS update) on operator panels? http://support.automation.siemens.com/WW/view/en/26437978 SIMATIC HMI HMI devices Basic Panels-> 5.1.8 Calibrating the touch screen http://support.automation.siemens.com/WW/view/en/31032678 OK this I try and a OS update and factory reset was completly performed. The problem persist, i can't calibrate screen, becose 2/5 crosses i can't see in screen calibration process. Please help to solve this problem, I am worried what would happend with my others KTP 400 in further times. Best Regards |
Follow us on