12/1/2011 9:01 PM | |
Posts: 11 Rating:
|
hi; What can be done to see the value of the timer is running KTP 400 panel |
12/2/2011 2:08 PM | |
Posts: 3037 Rating:
|
Hello, you can see in the following link,how you can set a timer over an operator panel. How do you specify the runtime for a timer via an operator panel, or how do you output the remaining runtime? Tweety |
12/9/2011 1:25 PM | |
Posts: 3037 Rating:
|
Hello, you can migrate this project to TIA Portal. Which behaviour do you have? STEP 7 Basic V11.0 SP1 WinCC Basic V11.0 SP1 Tweety |
12/11/2011 7:20 PM | |
Posts: 11 Rating:
|
Hi; I have STEP 7 Basic version10.5-sp2, the timer values for this version is also seen in the panel? |
12/12/2011 2:06 PM | |
Posts: 3037 Rating:
|
Hello,
I can not understand what you mean? Here is the manual of STEP 7 Basic version10.5. SIMATIC STEP 7 V10.5 SP2 Perhaps it can helps this FAQ. In STEP 7 Basic V10.5, how do you convert the number of days, hours, minutes and seconds into milliseconds? Tweety |
12/13/2011 9:31 PM | |
Posts: 11 Rating:
|
hi; KTP 400 tia portal version 10.5 program for the panel which tool can I see on the screen using the timer values |
12/14/2011 5:37 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, sorry, but i think "Tweety" have give you good sample for your problem. In the Attachment you will find a simple "WinCC flexible 2008 SP2" project. Maybe you can open this file. (If you have the right software!) There you can see what you have to do. (Note and look to the properties from the tags). -> I also did not have WinCC TIA V10.5 . I mean you should update to V11 !!! But hersome instruction: (I hope under V10.5 are the same setting as under V11) Timer: For the Input "TV" => The Tag_1 are from typ "S5Time". Under V10.5 you use also a Tag_1 from type "S5Time". For the output "BI" you use a Tag_2 from typ "Word". Under V10.5 you use also a Tag_2 from typ "Word". V10.5: Under the properiesfor the Tag_1 you use the "Linear scaling" "PLC End Value: 1000" "HMI End Value: 1" "PLC Start value: 0" "HMI Start value: 0" regards, AttachmentWinCC_flexible_STEP7_Timer.zip (123 Downloads) |
12/14/2011 8:34 PM | |
Posts: 11 Rating:
|
Thank you, the file review doing |
Follow us on