4/3/2014 11:58 AM | |
Posts: 4 Rating:
|
Thanks, it's a good idea, i try it with fixed values. I'm going to write. |
This contribution was helpful to
1 thankful Users |
4/3/2014 12:01 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hi derdani, Let us know the result |
4/8/2014 6:35 PM | |
Posts: 4 Rating:
|
Hello again, it's not about the wrong values of the variables, I'm sure. I've found a topic in the forum, where they posted the same problem what we have. I want to try their solution: "With a reset to factoy settings and an update of the Image with the Operating System, the HMI has been running without incidentes for 10 days." I have a question: what does the "update of the Image with the Operating System" mean? Is it equal to Update Operating System? A little note to the problem: When I turn off the PLC after the HMI lost the communication, the HMI shows the correct values again for a half sec. |
4/9/2014 8:46 AM | |
Joined: 4/24/2006 Last visit: 2/7/2025 Posts: 8839 Rating:
|
Hello derdani, Please have a look at the following link: how do you do an operating system update (OS update) on operator panels? Use the option "Reset to factory settings" Use the right cable: Which connector cables are available for connecting to SIMATIC Panels? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on