6/9/2011 11:04 AM | |
Joined: 1/28/2009 Last visit: 2/21/2023 Posts: 6794 Rating:
|
Check this: https://www.automation.siemens.com/mcms/human-machine-interface/en/operator-interfaces/basic-panel/simatic-hmi-ktp600-basic-color/Pages/Default.aspx?HTTPS=REDIR#Area%20of%20application |
6/9/2011 11:28 AM | |
Joined: 10/12/2007 Last visit: 1/1/2021 Posts: 64 Rating:
|
Hi, Thanks for the link. But it is not making me clear wheather this is suitable for using with S7-300R. I would like to use it with R so I guess that would require the C scripting for switching over of the connection. Does this HMI support the C scripting using which I can switch the connections? If so, is there standard script available for the same? Best Regards, |
Prashant VISPUTE |
|
6/9/2011 4:38 PM | |
Joined: 4/29/2010 Last visit: 3/30/2023 Posts: 1557 Rating:
|
Hello, basic panels doesn´t support scripts. best regards |
Follow us on