4/17/2016 7:07 PM | |
Posts: 52 Rating:
|
now i can connect it with TIA Portal but the yellow led still running , is it a problem ? and how can i solve it ? can i make factory restore ? |
4/17/2016 7:54 PM | |
Posts: 107 Rating:
|
As long as it's connected to your system there's no problem. regarding the factory restore, you need to have SIMATIC Prosave I have attched screen shots for clarification AttachmentProsave.zip (261 Downloads) |
This contribution was helpful to
2 thankful Users |
4/17/2016 8:28 PM | |
Joined: 3/28/2015 Last visit: 2/15/2025 Posts: 722 Rating:
|
Hello, Perhaps the following topics might help: |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
1 thankful Users |
4/17/2016 10:47 PM | |
Joined: 5/28/2008 Last visit: 2/12/2025 Posts: 4518 Rating:
|
Hello, Do you still can communicate with this SIMATIC panel via Ethernet port? I think there is something abnormal happen in this port! And I don't think that OS update or even reset to factory will solve this problem. You can try and tell us. But normally, reset to factory setting is not a solution in case of hardware problems. Here's in the following link, the meaning of the two leds comes with ethernet port http://avtech.com/Support/faq/225/what-the-ethernet-port-led-lights-mean-on-room-alert/ I think you can still use this panel with other interfaces MPI or Profibus. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
6/8/2016 1:04 PM | |
Joined: 8/21/2014 Last visit: 2/12/2025 Posts: 1036 Rating:
|
New question published by rarlabrador is split to a separate thread with the subject Establishing a connection between the HMI and the PC. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on