Industry Online Support
Technical Forum
9/30/2017 5:35 AM | |
Joined: 6/24/2016 Last visit: 8/13/2023 Posts: 1 Rating:
|
Hi folks! By mistake i have downgraded a KTP700DP panel and now it cant be seen via MPI. Also it lost the USB option in the communication options. I know it was my mistake but now i have to repair it. It was a KTP700 DP (6AV2 123-2GA03-0AX0) basic panel with a 13.00.01.06_02.01 image version. Now it has a 13.00.00.03_20.13 image version. I downgraded it via USB with the file (KTP700DP_V13_00_00_03.fwf) which comes with my TIA V13 upd6. As i stated before, no MPI/PROFIBUS, no USB... What can i do now? and how? Any help will be very appreciated... (For the record my original problem was exactly this)
AttachmentWord_29_09_2017 22_34_01.pdf (83 Downloads) |
Follow us on