11/4/2019 12:43 PM | |
Posts: 5 Rating: (0) |
Thank you. I will try to find it and check. |
11/4/2019 1:36 PM | |
Joined: 12/18/2014 Last visit: 1/15/2025 Posts: 34496 Rating: (4306)
|
Yes, you can create virtual buttons for switching etc. But you can not to use for switching physical inputs of the LOGO!. The CMK2000 you need, if you have the LOGO! want to connect to a KNX bus. Do you want connect theLOGO! with S7, you need devices with Profinet on the S7 side. |
This contribution was helpful to1 thankful Users |
Follow us on