4/11/2012 6:17 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello again , I have finished my previously proposed code for your requirement. I have tested the result of my codes with SIMULINK and they were identical, as you can see in attachment.Note,You have 5 adjustable parameters that can generate a totally flexible transfer function for you.I will upload the project as soon as possible, you can use the function (FB300) even you are not familiar with SCL. Please note: F---> as input signal Y--> as output signal A,B,C,D,E as coefficient of Laplace transform as shown in attachment. REST-> to reset calculation Interval--> Time between to succesive OB3X calls (T#100mS) [code]FUNCTION_BLOCK FB300 // Block Parameters VAR_INPUT // Input Parameters F:REAL; A:REAL:=1.0; B:REAL:=1.0; C:REAL:=1.0; D:REAL:=1.0; E:REAL:=1.0; INTERVAL:TIME:=T#1S; END_VAR VAR_IN_OUT REST:BOOL:=FALSE; END_VAR VAR_OUTPUT // Output Parameters Y:REAL; END_VAR VAR_TEMP // Temporary Variables END_VAR VAR // Static Variables // FNEW:REAL:=0.0; X1:REAL:=0.0; X2:REAL:=0.0; X1OLD:REAL:=0.0; X2OLD:REAL:=0.0; DELTA1:REAL:=0.0; DELTA2:REAL:=0.0; T_INTERNAL:REAL:=1.0; FOLD:REAL:=0.0; FNEW:REAL:=0.0; END_VAR // Instruction Section T_INTERNAL := (DINT_TO_REAL(TIME_TO_DINT (INTERVAL)))/1000.0; IF REST=1 THEN X1:=0.0; X2:=0.0; X1OLD:=0.0; X2OLD:=0.0; FOLD:=0.0; FNEW:=0.0; //REST:=0; Y:=0; ELSE FNEW:= F; DELTA2 :=((((D*(FNEW-FOLD))/T_INTERNAL)+(E*FNEW))- (C*X1OLD) - (B*X2OLD))/A; X2:= X2OLD + (DELTA2 * T_INTERNAL); DELTA1 :=X2; X1 := X1OLD + (DELTA1 * T_INTERNAL); X2OLD:= X2; X1OLD:=X1; Y:=X1; FOLD:=FNEW; ; END_IF; ; END_FUNCTION_BLOCK [/code] Best regards, Hamid Hosseini AttachmentLAPLACE_FORUM.zip (659 Downloads) |
This contribution was helpful to9 thankful Users |
4/11/2012 6:44 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello , And this is the project.SCL Source code is also provided.If you are not familiar to SCL,Only copy the "FB300" in your project and call it in OB3X. Note, time between 2 successive calls of OB3X is included in calculation so this time should be constant and provided for the algorithm in "Interval" input. Please, feel free to ask any question about the function.There are plenty of qualified members to help. Best regards, Hamid Hosseini AttachmentHD.zip (356 Downloads) |
This contribution was helpful to1 thankful Users |
7/13/2012 5:53 AM | |
Posts: 36 Rating: (1) |
after processed in PID block, how to make a transfer function 2/(4s+1) of plant in S7? thanks Firza |
7/13/2012 10:12 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello , Finally data related to solving ODEs published publicly here: Numeric Methods to Solve ODEs(Ordinary Differential Equations )For your case refer to "1-First Order Differential Equation"which FB1 written in SCL provide numeric solution to equation you have presented. Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 11/26/2014 11:35 AMLast edited by: hdhosseini at: 8/16/2015 4:57:12 PM |
|
7/13/2012 1:12 PM | |
Posts: 378 Rating: (73) |
Well done hdhosseini Thank you so much !!! . |
Last edited by: desmul24 at: 7/13/2012 1:17 PM |
|
This contribution was helpful to1 thankful Users |
11/18/2014 12:49 PM | |
Posts: 1 Rating: (0) |
Dear Marko; Can you also provide this simpler method for the first order?
|
Follow us on