Industry Online Support
Technical Forum
6/14/2010 2:24 PM | |
Posts: 16 Rating:
|
I made a test line-up with these parts:- PS 307 2A 6ES7 307-1BA00-0AA0 CPU 315-2DP 6ES7 315-2AG10-0AB0 /V2.0 FM3546ES7 354-1AH01-0AE0 Laser distance sensor SICK DME 5000-111 (SSI) All the parameters of the absolute encoder are all preset for SSI, I checked them all and it looks all right.The display of the encoder tells me that it is in the ready-to-operate state and receives a clock signal. It also displays the measured value in meters. HW-config is no problem. I can go online with de CPU and the FM card. I checked the properties of the FM card following the manual “First steps in commissioning FM354” from Siemens. Everything looks fine, and logical, until I do a test via the “startup” screen. When I move the sensor, the actual value in the startup-screen remains 0.000mm, but the value on the sensor display changes. This is the first time I work with SSI and FM354. I searched this forum for related problems with SSI, very interesting, but that didn’t work out for my problem. I tested with different parameters in DB1200 with the same result.I can’t determine what I forgot or did wrong… Thanks in advance. I added the machine data (DB1200) in attachment AttachmentMD_dme5000.zip (110 Downloads) |
Last edited by: O_Moderator at: 6/14/2010 8:08 PM |
|
Follow us on