Industry Online Support
Technical Forum
1/30/2013 3:12 PM | |
Joined: 12/5/2006 Last visit: 2/6/2024 Posts: 73 Rating: (4) |
We have an application where an FM450-1 is used to count from a 24V encoder, while the counting is running we should receive an input ( rising edge) that stores the count value for comparison. I have seen this entry on the web site http://support.automation.siemens.com/WW/view/en/6510748but it shows only the FM350-1 that exactly what I would like to implement is there an example to implement this solution to the 450-1. Thanks |
9/14/2016 12:04 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by ausutf is split to a separate thread with the subject FM-350-1 counter card, stop conveyor after five rotation. Best regards |
Follow us on