10/15/2024 1:13 PM | |
Joined: 1/21/2013 Last visit: 2/7/2025 Posts: 3524 Rating:
|
Hi, You can use the Layer.Visible property to change the visibility of a screen layer using scripting. However, this is only supported in V18. Your previous posts suggest that you are still using V17. If so, you need to change the visibility of each screen element, not the layer. Kind regards |
10/18/2024 1:29 PM | |
Joined: 8/3/2009 Last visit: 2/7/2025 Posts: 14670 Rating:
|
Hi Stefan I think it works also in V17... I used it in a Unified comfort Panel project in TIA V17: Bye Murof |
If this Information really helps, you could use the Rate function |
|
10/21/2024 7:11 AM | |
Joined: 1/21/2013 Last visit: 2/7/2025 Posts: 3524 Rating:
|
Hi Murof,
Yes, you are right. The WinCC Unified Object Model in V17 already supports the "Layer" object. So it is possible to access it with scripting, but it is not yet supported to access it as a property within engineering. Kind regards |
Follow us on