6/26/2023 10:20 AM | |
Joined: 7/25/2014 Last visit: 9/20/2024 Posts: 21 Rating: (0) |
Hi Probably too late but here it is for Unified: https://support.industry.siemens.com/cs/ww/en/view/109813055 I am testing using it with Unified Runtime on a PC and it seems pretty good, the only thing that would stop me is the amount of powertags used. I tested using the faceplate and blocks for LBP_Mtr - Simple Motor. I looks and works very well but what is puzzling me is the PowerTags I am using for this single motors is 66 PowerTags? If I will implement everything in the plant using LBP the tag count will be enormous and I will need a huge license for a relatively small plant. Normally we use 2 tags for a simple motor. Am I doing something wrong or is there a way to do this with a "normal" amount of PowerTags? Good luck ------------------------------------------------------------------------------------------ |
Last edited by: Iccceman at: 06/26/2023 10:28:03Last edited by: Jen_Moderator at: 06/26/2023 12:15:49Link optimized. Last edited by: Jen_Moderator at: 06/26/2023 12:17:24New subject after splitting |
|
6/26/2023 12:18 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Library for Basic Processis (LBP) Powertags used for Unified Runtime is published within the conference WinCC Unified Systems. Jen_Moderator |
Follow us on