9/5/2006 7:54 AM | |
Posts: 3149 Rating: (171)
|
Hi, yes, this should work.... http://support.automation.siemens.com/WW/view/en/21927773 I´d advice to install the latest WinCC SP http://support.automation.siemens.com/WW/view/en/22303359 Here you can find the WinCC getting starteds and manuals: http://support.automation.siemens.com/WW/view/en/17356933 http://support.automation.siemens.com/WW/view/en/21320307 http://support.automation.siemens.com/WW/view/en/15343333 nemo |
9/7/2006 4:53 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
Have you seen these FAQs : - http://support.automation.siemens.com/WW/view/en/21914005 (mentions that you need the Object Manager installed) - http://support.automation.siemens.com/WW/view/en/11916587 - http://support.automation.siemens.com/WW/view/en/16522013 (PCS7 faq but may contain useful hints) |
9/8/2006 8:49 AM | |
Posts: 3149 Rating: (171)
|
Hi, in PCS7 the term "OS" (Operator Station) means WinCC ... => include your WinCC project there nemo |
Last edited by: Nemo at: 9/8/2006 8:50 AM |
|
9/8/2006 1:24 PM | |
Posts: 3149 Rating: (171)
|
Hi, unfortunately it´s not clear to me, why this option is greyed.... How did you install the simatic Software?? It´s recommended to install first STEP7 and then WinCC. if you should decide to deinstall, I´d deinstall STEP7 and WinCC inlcude the corresponding regkeys http://support.automation.siemens.com/WW/view/en/189025 nemo |
9/8/2006 2:04 PM | |
Posts: 1275 Rating: (123) |
Also... You're using Step7 5.3, but with which sp? |
9/8/2006 4:14 PM | |
Joined: 1/22/2006 Last visit: 10/8/2020 Posts: 73 Rating: (0) |
it is V5.3+HF2 |
Follow us on