10/13/2009 12:21 PM | |
Posts: 118 Rating: (4) |
Hi All, We are using MP277. We have created one project in Wincc Flexible 2008,SP1 and downloded to the MP277. We have the Wincc with Licenced one in our PC. After we downloded, more frequently we are getting the message in the MP277 that " SIMATIC Wincc flexible 2008 SP1 Runtime Licence Key not available!, SIMATIC WINCC Flexible/Sm@rtService for SIMATIC Panel". Is there any Licence Key required for MP277?...... |
10/13/2009 2:13 PM | |
Joined: 4/3/2008 Last visit: 4/22/2024 Posts: 385 Rating: (16) |
You don't need the license for the runtime while you are working with Siemens panel, but for Flexible/Sm@rtServiceor some other additional functions. Finally, there is no way, you have to buy. pigroplc |
This contribution was helpful to3 thankful Users |
10/13/2009 2:31 PM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Dear Maha, Only when you want to use Sm@rtAccess or Sm@rtService, you will need a license. Please check in WinCC flexible project -> Device settings -> Device settings Have you ticked the one of the Runtime services (Example:'Start up Sm@rtServer') Best regards, Wizard |
This contribution was helpful to2 thankful Users |
10/19/2009 4:02 AM | |
Posts: 118 Rating: (4) |
HI Wizard, Thanks for your support. We have not done any additional settings in Device Settings. I have attached the Device Settings Screen Shot for your reference. One more important things that, we are not required to use any runtime services in MP277. AttachmentDevice_Settings.pdf (565 Downloads) |
Last edited by: Maha at: 10/19/2009 7:45 AM |
|
10/19/2009 9:03 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, did you have use the panel beforefor a nother project? Maybe you should make a OS Update with "Reset to factory settings" -> http://support.automation.siemens.com/WW/view/en/19701610 Or delete all temporary files under "Options" (flexible 2008). Furthermore you cansave the project under a new name. regards, |