6/28/2016 1:44 PM | |
Joined: 7/1/2014 Last visit: 3/18/2024 Posts: 230 Rating: (24) |
Before formatting the PC, did You transfer back to the USB the licenses? If not, these are lost during the format of the PC... If that is the case, you should contact Siemens, and with the serial code con the USB stick of the License You should be able to obtain a new license for free by them... but anyway You should contact them and find out what they need to grant you a new license in substitution of the one You lost formatting. You should also have the CoL (Certificate of License) that Siemens gave you when You buyed the license, there it is also the information they need to recover your licenses. If You want to activate trial license maybe thiscould be of help: https://support.industry.siemens.com/tf/ww/en/posts/tip-step7-v12-trial-how-to-enable-the-trial-license/88304/?page=0&pageSize=10 |
Last edited by: dan.v. at: 6/28/2016 1:46:32 PMLast edited by: dan.v. at: 6/28/2016 1:47:02 PMLast edited by: dan.v. at: 6/28/2016 1:53:25 PMLast edited by: dan.v. at: 6/28/2016 1:53:43 PM |
|
This contribution was helpful to1 thankful Users |
6/28/2016 1:55 PM | |
Posts: 11 Rating: (0) |
it was working this morning. after i changed pc time, i started not to work. here is photos in a pdf file. should i format pc again?Attachmentphotos.pdf (252 Downloads) |
Last edited by: Ltsc at: 6/28/2016 1:57:54 PM |
|
6/28/2016 2:28 PM | |
Posts: 11 Rating: (0) |
i'm an intern not an employee. i'm trying to learn scada systems. thanks chris. |
4/9/2018 10:49 AM | |
Joined: 4/9/2018 Last visit: 5/23/2019 Posts: 1 Rating: (0) |
We have problemms to donwload licence file because the link is expired, |