7/14/2019 7:12 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, I have a small issue with the circuit attached,it works ok until input 4 is switched i would like to keep Q2 energized, What i am looking to achieve is hob switch brings in both fans which it does.The light/fan switch brings in bathroom fan and light which it does,but when both fans are running and the light/fan switch is energized the fan (Q2) goes in the off state I would like to avoid this Ade Attachmentmultiway_switching_circuit_v8.zip (128 Downloads) |
7/14/2019 7:31 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
It is exactly what I was looking to achieve Thank you so much.... |
This contribution was helpful to1 thankful Users |