11/21/2014 7:42 PM | |
Joined: 9/20/2010 Last visit: 11/11/2021 Posts: 6 Rating:
|
Dear Expert, We have installed 900 kW MV 690 drive (560 kW x 2 modules) along with Line Harmonic Filter. There was some recomendation by client to accomplish LHF. But we got very surprised that enery meter (multi function meter) installed in MV breaker shows heavy current draw while drive/motor not even running. This drawn current varies from 240 amperes to 250 amperes while in load run time total current could be 600 to 940 ampere depend on load. (Motor full load is 940 ampere). we have checked current from clamp meter & it really shows same. How we can avoid this huge loss for nothing.Is it drive configuration mistake or what, I am attaching SLD also. LHF type : 6SL3000-0JH35-8AA0 SINAMICS G130 Drive Converter Chassis Unit : 6SL3310-1TH35-8AB3 Please help. Thanks. Regards Santosh Verma AttachmentSLD of 541MD1_900 kW.pdf (86 Downloads) |
Follow us on