8/23/2018 10:20 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 112 Rating:
|
Hi Yu-Wen, Tested the initial program as the last modified program which we had with TCON had some errors when I pressed PUBLISH. After a long struggle finally I am able to transmit the data's to and from the mosquito MQTT Server using TIA Portal V15. Now I am at the final stage, I need to connect to an online free dashboard to connect it to my PLC. I am using a online free "Freeboard.io". I am facing few difficulties while linking the server to the dashboard. Below are my entries, PLEASE ADVICE ME ON THE CONNECTIONS; 1. TYPE : MQTT 2. NAME : ( Any name ) 3. TOPIC : qwerty ( Advice ) 4. SERVER : 37.187.106.16 ( Advice ) 5. PORT : 1883 6. USE ENCRYPTION : NO 7. CLIENT ID : mqttdemo ( Advice ) 8. API KEY / USERNAME : steve 9. PASSWORD : john 10. JSON MASSAGES : no I have attached the screen shots for your reference please advice. Thanks Regards Satheesh ------------------------------------------------------------------------------------------ Attachmentmqtt.zip (38 Downloads) |
Last edited by: Jen_Moderator at: 8/23/2018 1:27:40 PMNew subject after splitting Thanks |
|
Follow us on