6/1/2011 4:19 AM | |
Joined: 5/31/2007 Last visit: 2/28/2025 Posts: 90 Rating:
|
Hello, my men : File attachmet. I installed STEP7 V10.5 in a notebook, and I use a Ethernet cable(RJ45) connection notebook and S7 1200 without using aSwitching HUB. But I can't scan any IP in th "Accessible devices" icon, even if I set specific IP for example 192.168.1.1 in the notebook Ethernet card, I still can't scan and display any IP in STEP7 Basic V10.5, so I couldn't do upload and download in the further steps. Any possible lead to this problem, and please give me some suggestions. Thanks a lot. AttachmentConnection_Error_PIC.zip (85 Downloads) |
6/1/2011 5:33 AM | |
Posts: 212 Rating:
|
hi Which type of IE cable are u using? Straight or Crossed? you must use Cross cable if you are working w/o scalance. |
6/1/2011 6:24 AM |
|
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
hello, |
VANDE MATARAM..... |
|
6/1/2011 8:18 AM | |
Posts: 691 Rating:
|
Dear SexDriver Please use manual IP Address Setting. Also follow the above mentioned posts. |
6/1/2011 8:14 PM | |
Posts: 947 Rating:
|
Hi modern Profinet CPU have autocrossover properties. Connect to network computer and with utilitiesPing check each node. May be IP node same IP routers? |
Follow us on