6/28/2015 1:46 PM | |
Posts: 6 Rating:
|
Hi, I am using OBA8 controller and it is powered on 24X7 and would like to log the input and output data contineusly. when i tested it on my controller it was giving me good results untill there is a power failure. once the power failure occurs it starts giving me odd values. i had attached the excell file which shows the values given by PLC And I would like to inform you that there is no initialisation button present in the circuit because it should be up and running as soon as the power resmes. Thanks in advance. Attachment192.168.1.200_2015-6-19 15-22-2.xlsx (64 Downloads) |
6/29/2015 10:21 AM | |
Posts: 6 Rating:
|
Please find the circuit diagram attached
AttachmentCircuit Diagram log test.rar (66 Downloads) |
Follow us on