2/8/2019 3:51 PM | |
Joined: 8/3/2009 Last visit: 5/24/2024 Posts: 12981 Rating: (1653)
|
Hello Which Device do you use??? Only an Advanced Runtime can use 500000 entiries per log. If you have a Comfort Panel then you should not use more than 20000 or 50000, it depends on the device type. If this is to less for you then check this out: https://support.industry.siemens.com/cs/de/en/view/109477071 If you have a WinCC Professional Runtime than size or amount of entries are no Problem... Bye Murof |
If this Information really helps, you could use the Rate function |
|