Industry Online Support
Technical Forum
2/14/2013 4:53 PM | |
Posts: 3037 Rating:
|
Hello, Which Runtime do you use? Advanced or Professional? Tweety |
2/16/2013 6:42 AM | |
Posts: 515 Rating:
|
Hi Tweety, Am using Wincc advanced v11 sp2.
|
2/18/2013 4:22 PM | |
Posts: 3037 Rating:
|
Hello, This is the description of WinCC flexible: Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? If you want start your project directly? You need the pdata.fwc file of your project. You find it under your projectfolder --->IM --> HMI ---> ...... You can start your project about the RT Loader. Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on