4/16/2009 5:05 PM | |
Joined: 9/23/2005 Last visit: 8/27/2024 Posts: 4347 Rating: (1442) |
Hi, I wrote a article, that was not yet converted to a FAQ. Here is the preliminary version. The Stacker FB does these work to you. AttachmentSTEP 7 Staker.zip (1182 Downloads) |
Last edited by: Pegaia at: 8/3/2010 3:52 PMminor corrections on the documentation Last edited by: Pegaia at: 2/10/2010 11:05 AMProgram corrected Last edited by: Pegaia at: 2/9/2010 3:37 PMBug detected: Pay attention on Extract_At_Position function: Everything works as long as I extract double words from position 1, but if i extract from position 2, the number of entries in buffer decreases with 1, but the data in the buffer doesn''''''''t shift. I changed line 444 in the scl source, from this "x1 := nr_DBD_to_move * 4 - 4;" to this "x1 := nr_DBD_to_move * 4;" As soon as possible, I will correct it. Denilson Pegaia |
|
This contribution was helpful to6 thankful Users |
4/17/2019 2:19 PM | |
Joined: 5/22/2009 Last visit: 5/3/2022 Posts: 40 Rating: (0) |
There is a version for TIA portal V14 ? Or just project conversion works ? Regards |
12/26/2019 4:54 PM | |
Joined: 9/23/2005 Last visit: 8/27/2024 Posts: 4347 Rating: (1442) |
Hi, here there is a V13 SP2 version of it. I think you can open it on V14 too. AttachmentProject4.zip (239 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on