11/16/2018 11:19 AM | |
Joined: 12/18/2014 Last visit: 12/3/2024 Posts: 34325 Rating: (4276)
|
The astronomical clock calculates due to the parameters: I can not say more about that either. But if you want to have an official statement, then start a Support Request. |
11/26/2018 8:31 AM | |
Joined: 9/11/2014 Last visit: 12/2/2024 Posts: 782 Rating: (33) |
Hi, does anyone else has access to your LOGO!? Please upload your program so we can have a look. Regards Helmut |
12/5/2018 6:14 AM | |
Joined: 12/27/2006 Last visit: 11/29/2024 Posts: 1197 Rating: (113) |
Is there an micro-SD cart in your LOGO? And is the programm (also) on that SD-card? |
12/17/2018 9:05 PM | |
Posts: 32 Rating: (0) |
Hi... Maybe the logo! hardware is faulty... |
Follow us on