4/30/2021 7:31 PM | |
Joined: 4/14/2013 Last visit: 3/12/2023 Posts: 27 Rating:
|
Hello. You have get solution? If not: Check , what of version Win 10 you have (32bit or 64bit). Is that new version LOGO! Soft Comfort 8.3 compatible to your computer. Check , what is the instalation location of installed "LOGOComfort_V8.3" (like: C:\Program Files\Siemens\LOGOComfort_V8.3) and then, the shortcut properties what you use, it points to a right startup file (like: C:\Program Files\Siemens\LOGOComfort_V8.3\LOGOComfort.exe). I have both versions of them on the computers and both working. I have experienced Win 10 Pro installed software under one user, will run sometimes halfway from another user . Hope this helps. |
Last edited by: Jen_Moderator at: 05/03/2021 10:03:03Optimized link. |
|
5/3/2021 7:00 AM | |
Joined: 9/11/2014 Last visit: 12/8/2023 Posts: 680 Rating:
|
Hi, there was a similar post in the past. Here how they have fixed it: Hope this helps |
5/28/2021 9:16 AM | |
Joined: 12/18/2014 Last visit: 12/9/2023 Posts: 31592 Rating:
|
On my PC are installed different versions of TIA and different versions of LSC. No problem. |
Follow us on