7/19/2017 5:21 AM | |
Posts: 5 Rating: (0) |
I have a LOGO 8! FS4 LOGO SOFT 8.1v y SIMATIC S7 1200 1214 AC / DC / RLY with firmware 4.2 TIA PORTAL 14V. I try to connect but nothing happens, S7 not receive anything . the communication doesn't work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/19/2017 8:23:33 AMNew subject after splitting |
|
5/31/2018 2:00 PM | |
Posts: 6 Rating: (1) |
I just did the same exercise, and It doesn't work. Like you I have a LOGO FS4 and 1200 V4.1. Please, we need a solution! |
6/4/2018 11:20 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 7995 Rating: (163) |
New question published by frantam is split to a separate thread with the subject Data writting from S7-1200 to logo NOT work. Best regards |
My Forum is the place to personalize your profile, |
|
6/18/2018 9:17 PM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32943 Rating: (4072)
|
Create the connection with the LOGO! as a client and the S7 as a server. In TIA: AttachmentScreenshots.zip (541 Downloads) |
This contribution was helpful to1 thankful Users |
6/19/2018 9:34 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
Hello all logo is DB1.BDXzzz when zzz is adress in logo memory. Active connection establishment is enable. Read and write works fine. If logo write connection error and red backlight help me changed TSAP. Tsap is it posible changed if added new S7 connection in logo this connection incremet TSAP and old connection may be deleted. FrantaM Attachments7%20logo8%20put%20get.zip (338 Downloads) |
6/19/2018 9:48 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
Yes it is true. |
Follow us on