4/4/2015 12:29 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215) |
Does your logo a display? If so, then you can see yourself. In the Network menu> Ip address. |
4/4/2015 1:05 PM | |
Posts: 24 Rating: (0) |
I tried to do this, but putting the last IP address does not start the connection, possibly the Logo Confort must have changed the ip of the logo |
4/4/2015 5:09 PM | |
Posts: 24 Rating: (0) |
I did this test but does not work. with the TDE can not give any commands to the logo |
4/4/2015 8:16 PM | |
Posts: 24 Rating: (0) |
I solved the problem was caused by the network card of the PC. thank you all
|
This contribution was helpful to2 thankful Users |
4/4/2015 9:05 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215) |
Thanks for the Feedback. |
Follow us on