5/30/2012 7:39 PM | |
Posts: 22 Rating: (0) |
Have ticked the box to display message on both LOGO! and LOGO! TD in the message text SFB properties? |
5/30/2012 8:22 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (581)
|
Hello, it gives different firnware versions of the TD: ES6 ist full compatible with the 0BA6 AND ES7 ist full compatible with the 0BA7 but - TD with ES6 can work with 0BA7 but only Parameter up to block nummber 200 can displayed and only values and parameters of block typs from the 0BA6 can displayed.. To display values of the block astroclock you need a TD wir newest firmware Sorry... Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to1 thankful Users |
5/31/2012 8:22 AM | |
Posts: 5 Rating: (2) |
Thanks for the responses guys. |
This contribution was helpful to1 thankful Users |
Follow us on