11/3/2014 3:42 PM | |
Joined: 11/23/2011 Last visit: 10/4/2023 Posts: 202 Rating:
|
Hello Liudas, when installing an LOGO!Soft Comfort upgrade with Windows 7 you have to take care that you execute the files as administrator. I would try to follow the steps in this FAQ: Why does an error message appear when installing an update/upgrade for LOGO!Soft Comfort in Windows 7? If you have still the problem please try to upgrade manually or via the update-center following the instructions of this two FAQs: How do you install a downloaded upgrade for LOGO!Soft Comfort with or without installed LOGO! software? With LOGO!Soft Comfort how do you make an upgrade, update or extension via the Update Center? The FAQs above reference to upgrade of LOGO!Soft Comfort to version 7.1 but it doesn't matter, you can use the same installation way also for upgrade to LSC V8. I hope you get the solution soon. Greetings, KM_AS |
11/4/2014 6:45 AM | |
Posts: 9 Rating:
|
finally after about 20 times of trying update through internet it completed. Thanks for help
|
6/7/2019 3:37 PM | |
Joined: 2/7/2019 Last visit: 12/6/2023 Posts: 1 Rating:
|
Hello where can i find the download for updating from v7 to V8 someone thanks Patrick |
6/7/2019 4:55 PM | |
Joined: 12/18/2014 Last visit: 12/11/2023 Posts: 31596 Rating:
|
Hello patrickd83, at first welcome to the forum. Forget the link in the post above from the user Wizard. On the linked web site there are no more updates or upgrades for LSC. Siemens makes a new way. A upgrade a the current version of LSC (V8.2.1) find you here: Notes on instructions for updating the LOGO! 8.2 SP1 operating System But is a big download package (1,3 GB). It is with - upgrade of LSC And the download is export restricted! You need a additionally registration for this software. |
This contribution was helpful to
1 thankful Users |
Follow us on