Industry Online Support
Technical Forum
1/16/2012 10:06 PM | |
Posts: 133 Rating: (13) |
Hello, Sorry I do not have a sample program but this function could easily be accomplished with the traversing task in the basic positioner of the S110 or S120.First you start the drive, then you enable the traversing function in the postioner. You only need two of the traversing block to do this task. The first block command calls for endlessmovement (positive or negative direction commands available)at the specified velocity until the external input is active. The next block is a relative position call the distance you want to move. The details would be in the Closed Loop Position control in the Function Manual (FH1) or STARTER help under Traversing Blocks. AttachmentDoc1.pdf (252 Downloads) |
Last edited by: Drives_Coach at: 1/16/2012 10:12 PM |
|
1/16/2012 11:21 PM | |
Posts: 5 Rating: (0) |
Thank you Drives_Coach. I will make this work with your guidance. Have an excellent day! |
Follow us on