8/3/2015 9:23 AM | |
Posts: 211 Rating: (6) |
Hi! I use TIAP V13 SP1 Upd4 professional, And switch which is not in catalog is XB205-3LD. |
Last edited by: Homeroid_BL at: 8/3/2015 9:32:50 AM |
|
8/3/2015 9:48 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hmm... didn´t found anything. But it´s very new(one month). do you have the newest HSP? |
FCK WAR! |
|
8/3/2015 9:56 AM | |
Posts: 211 Rating: (6) |
Yes, I do. |
8/3/2015 10:07 AM | |
Posts: 211 Rating: (6) |
Swich will be here in a month, but I must finish project BEFORE switch arrives, and install it immidiately |
8/3/2015 10:10 AM | |
Posts: 211 Rating: (6) |
And, how it is that my project's communicaton partners of XB205-3LD, switches XB004-1LD ARE IN HW CATALOG? |
8/3/2015 10:14 AM | |
Posts: 211 Rating: (6) |
How can I program Put/get data exchange, since swithes are not in topology, and I can not make physical connections which means no logical connections? |
Follow us on