4/4/2020 12:31 PM | |
Joined: 3/27/2009 Last visit: 2/11/2024 Posts: 92 Rating: (6) |
Hi there, That is exactly what is a part of my next extension of my home project. i have a diesel tank and two LPG tanks, (i am off grid), The LPG tanks are for heating and cooking. The 2 tanks are a 40 Meters from my house close to my diesel tank and generator, so inspection from within the house will be nice. I was already checking what type of sensor i can use and you have given a nice idea. At the generator i already use a LOGO PLC networked to the house. I include the data sheet for what i understood is your sensor. I have setup a small diagram that works with a trigger to have a minimum level at the input and then a short delay for stable signal. This will enable a threshold to keep the output at the last level. This is NOT a finished diagram but i think a nice step in the correct direction. P.s. keep in mind the LPG tank is never filled 100% with liquid to keep a evaporation space. AttachmentLPG tank level (2).zip (183 Downloads) |
Last edited by: Peterako at: 04/04/2020 12:37:23 |
|