12/1/2011 7:26 AM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715) |
Hello, Well, you have to study the manual and the local regulations. Have here 1 manual, there are lots more, don't know the exact type you have in mind. http://support.automation.siemens.com/WW/view/en/38741858 Have a close look at the Environmental part of it. Regards, Marcjan |
Last edited by: Marcjan at: 12/1/2011 7:28 AMProblem solved? |
|
12/3/2011 12:27 AM | |
Joined: 11/1/2007 Last visit: 5/22/2024 Posts: 36 Rating: (0) |
Thanks |
12/12/2011 10:31 AM | |
Joined: 11/1/2007 Last visit: 5/22/2024 Posts: 36 Rating: (0) |
Is it safe also use LR250 on same closed vessel 9% alcohol content, 20 inH2O pressure? Thank you so much |
12/12/2011 3:00 PM | |
Posts: 74 Rating: (3)
|
Hi Again habella Sure it is. Just make sure you select the correct area electrical classification and heed the warnings I posted earlier. Note that 20" H2O pressure is less than 0.5 atm so you will not require a pressure rated version. This saves a few $$. Build your LR250 on the PIA Selector http://pia-portal.automation.siemens.com Cheers [ |:) |
Follow us on