9/4/2018 10:54 PM | |
Joined: 7/25/2017 Last visit: 3/13/2025 Posts: 355 Rating:
|
Hi, I have a M876-4 set up for Sinema RC. The CLI config dump is attached. In some locations it works fine and I have done extensive PLC modifications in TIA Portal over VPN. But in other locations, we get some interesting behaviour. Here is my problem: it seems to connect to cells not belonging to the PLMNID of my provider (53005), which do not provide internet access. As per the CLI config dump, I have two providers configured, Manual and 53005. But Manual is disabled. Therefore, my understanding is that it should only try to connect 53005. Has anyone faced a similar problem and/or know what might be happening here? AttachmentRunningCLI.txt (118 Downloads) |
Follow us on