6/18/2010 7:01 AM | |
Joined: 9/18/2006 Last visit: 5/3/2024 Posts: 589 Rating: (64) |
Hi DEEPSTR2010. Excuse me. You are right. All it is in the documentation on commissioning. Probably I repeat. Best regards. AttachmentParameterize axis data.pdf (222 Downloads) |
6/18/2010 7:27 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
HI pfuser, Thank you for your valuable information. Regards, DEEP. |
6/18/2010 7:30 AM | |
Posts: 43 Rating: (2) |
hi deep, Motor 100 RPM, pinion RPM is 1 which is equal to linear travel = 400 mm. It's correct Y.Dhinakaran. |
6/18/2010 7:54 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello Dhinakaran, Thanks for the confirmation. Regards, DEEP. |
6/18/2010 8:31 AM | |
Posts: 43 Rating: (2) |
hi deep, here is the described mechanical gear ratio chart and its explanation. Y.Dhinakaran. AttachmentGEAR RATIO CHART.pdf (175 Downloads) |
6/20/2010 7:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hi Dhinakarn, Good Morning. No yet the problem isn't solved. As discussed in forum we tried by varing different parameters & by adjusting gains, but of no use. Little bit improvement is their but not to satishfaction level. Since machine is lathe machine & application is of finish turning Z axis must run smoothly i.e. without jerk/vibration. At present we have opened up slide & checking for any mechanical probelm. After completion & confirmation of mechanical functioning, we shall check up & let you know. Meanwhile attaching here with Z axis parameter file FYI pls. Regards, DEEP. AttachmentZ axis parameters.pdf (198 Downloads) |
Follow us on