9/30/2015 1:58 PM | |
Joined: 4/28/2015 Last visit: 4/18/2024 Posts: 11 Rating: (0) |
Greetings to all, I have come across a similar issue so I thought that I should continue on this thread. About 20 units of MAG 800 flow meters with GSM/GPRS comm card have been installed in a site. So far we have managed to configure them so that the metering data arrive to a PC with Siemens MAG 8000 OPC Server installed. The data are saved as .CSV Files but as they are starting to be too many to handle we are required to directly link them to an existing SQL Database. The manual states that incoming data are automatically stored in an sqllite database but there is no mention of the path that the database is stored. Does anybody have an idea of where the sqlite database files are? Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/30/2015 2:24:21 PMNew subject after splitting |
|
1/19/2016 11:43 AM | |
Joined: 12/11/2012 Last visit: 6/7/2023 Posts: 34 Rating: (10) |
%APPDATA%\Siemens\MAG8000 OPC Server\Database\mag8000.sqlite |