5/26/2011 4:14 AM | |
Joined: 3/28/2010 Last visit: 10/1/2023 Posts: 977 Rating:
|
You have a maximum flow of 1200 gpm and you want a maximum flow rate of 1500 gpm.
You need to re-range the settings on the 5000 so that 20mA becomes your maximum flow (1500 gpm) rather than the 1200 gpm it is set to now. That can be done as long as your mag tube (the sensor in the pipe) will support the higher flow range.It isn't possible to determine from the information you provided whether that's the case or not, but give it a try and see. This quote from the 5000 manual describes the some of the setting involved (measuring range):
|
Follow us on