5/19/2011 4:41 PM | |
Joined: 5/28/2008 Last visit: 3/26/2023 Posts: 4390 Rating:
|
HelloEvertonf, The Prosave software is used to take a backup and restore the application software without modifing any thing in that application software and under a condition of using the same part number of the panel. That means that you have to restore to TP170 A. I know that TP170A is obsolete, and if the Programmer of the TP170A did not marked the check box of back transfer, so you have to ask him about the original software and open it with WinCC flexible and change the device to TP177A. If you can not get the software, then you have to begin of programming the TP177A from scratch. Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
5/19/2011 4:58 PM | |
Posts: 3 Rating:
|
Hi, I bought a new HIM, because the 170A was discontinued, I can remake the backup HMI 170A, and restore in the HMI 177A with WinCC flexible. Regards. |
7/17/2017 2:16 PM | |
Joined: 6/19/2017 Last visit: 3/27/2023 Posts: 6680 Rating:
|
New question published by Antony_BR is split to a separate thread with the subject Backup come in format .brf - How open this backup?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on