5/29/2020 10:33 AM | |
Joined: 1/24/2014 Last visit: 1/10/2025 Posts: 127 Rating:
|
Hi It seems you are trying to make a "self-made pop-up" First idea, use the integrated pop up with a faceplate in it (the faceplate is NOT the popup) As you open the pop up, you update the properties of your faceplate You can add a button (increment + decrement) or an IO field (with text list) to navigate between your different analog in your Pop up > I will choose this solution Second idea, make you own pop-up, and use script (inside the faceplate) to modify visibility of every object in the faceplate https://support.industry.siemens.com/tf/ww/en/posts/move-two-faceplates-in-wincc/237592/?page=0&pageSize=10 |
This contribution was helpful to
1 thankful Users |
6/1/2020 8:27 AM | |
Joined: 8/1/2012 Last visit: 11/13/2024 Posts: 76 Rating:
|
@sixthomas. Thanks! I will look into it. @Murof, I'm using this for comfort panel Regards, wantutri |
11/23/2020 2:39 PM | |
Joined: 6/11/2018 Last visit: 3/31/2022 Posts: 7 Rating:
|
if i know correctly then use of UDT is not allowed in VB script |
Follow us on