6/13/2018 9:31 AM | |
Joined: 1/9/2017 Last visit: 7/15/2021 Posts: 2 Rating: (0) |
Hello good day! Our system currently runs at a PCS 7 version 7.0 and we want to upgrade it to the latest version which is 9.0. I was about to check the links given above on how to update PCS 7 but it seems that the links given by jumo and Heisenberg_ has no information on it. Any information regarding steps and procedures about PCS 7 upgrade is very much appreciated. Thank you very much! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/14/2018 1:46:27 PMNew subject after splitting |
|
6/14/2018 2:06 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello Kurt Maynerd, please have a look at the booth manuals: SIMATIC Process control system PCS 7 Software update with utilization of new functions. SIMATIC Process control system PCS 7 Software update without utilization of new functions |
Last edited by: Thunderstorm at: 6/14/2018 2:07:37 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
6/14/2018 2:29 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello Kurt Maynerd, the latest version is PCS 7 V9.0 SP1. If you buy PCS 7 V9.0, you get the version V9.0 SP1. If you have bought PCS 7 V9.0 a few weeks ago, you can order the SP1. If you do a migration, it is recommended to use the newest Service Pack. PCS 7 V9.0 SP1 - Readme
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
10/1/2018 4:10 AM | |
Joined: 1/9/2017 Last visit: 7/15/2021 Posts: 2 Rating: (0) |
Thank you very much Thunderstorm. This is very helpful. Regards. |
Follow us on