1/21/2010 1:19 PM | |
Posts: 17 Rating: (0) |
i know the basic of plc ladder. |
1/21/2010 3:32 PM | |
Posts: 382 Rating: (47) |
Hello sumair, Well, these 2 are considered big topics. Perhaps the following linkscould help you. It is good to know some basic/common hardware of siemens PLCwhich I think this could in return help you in doing programming. Of course you also need know how to use or familiar withsiemens step7. 1] SIMATIC S7-300 S7-300 Module data 2] SIMATIC S7-400 S7-400 Automation System Module Data 3] Programming with STEP 7 V5.4 4] Ladder Logic (LAD) for S7-300 and S7-400 Programming 5] WinCC V6.0 Basic Documentation 6] WinCC: Working with WinCC 7] WinCC V6.2 Getting Started 8] SIMATIC V7.0 SP1 Getting started The above could be a good startfor you to explore the gist ofsiemens PLC & Wincc. To really know deeply for these two bigtopics, you need to play with them alot and accumulate your experience through projects (& maybe some bedtime reading). In future, if you are hungry for more and deeper knowledge, come to the forum again!. This is a good knowledge sharing place!. There are lots of members/experts which I am sure will be willing to help you and share their knowledge & experience with you! Hope this helps! with regards, how come |
Last edited by: how come at: 1/21/2010 3:41 PM |
|
This contribution was helpful to1 thankful Users |
1/21/2010 5:48 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
You can look for books from Hans Berger: e.g: http://www.amazon.com/Hans-Berger/e/B001JOPGC8/ref=ntt_dp_epwbk_0 |
|
|
This contribution was helpful to1 thankful Users |
1/21/2010 9:38 PM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
Hello Sumair, As you can see the gentlemen had already given you links for books and manuals. You can also look at the videos linked in this thread which may form an intermediatestep between the basics of PLC LAD and the STEP7. All PLCs might look the same when it comes to basic LAD instructionsbut stillthe operating system of the PLC differs from one brand to another. I recommend to concentrate on understanding of PLC operating system(S7 CPUs)which is simply explained in these videos. Best regards. H-H |
This contribution was helpful to1 thankful Users |
6/15/2010 8:25 PM | |
Posts: 6 Rating: (0) |
thank you for this manual |
Follow us on