2/27/2017 6:10 PM | |
Posts: 116 Rating:
|
Dear Members, I migrated a project from OP 270"Protool" into OP 277 "WinCC Flexible 2008 SP2" then into OP 277 "TIA V 11 SP2" then "Resize screen" and change the panel into KP700 After we finished the migration into KP 700,we faced 2 problems: 1-Some shapes distorted due to missing some vertical lines. and use "Resize screen" without benefit. 2-Not able to map the K functions to KP 700 as exist in old panel OP 270 and explanation PDF not help me to know the procedure. What is the procedure for mapping K functions to KP 700 ? How can we solve these problems. Thank you in advance. AttachmentMapping of the soft key assignment.pdf (210 Downloads) |
2/27/2017 7:08 PM | |
Posts: 5225 Rating:
|
Regardless if you believe in Karma or not. Bad Karma sure does believe in you. No user or picture change helps.. you'll have to dig deeper. Murof is by far the best person to answer you. I will reply on THAT thread what I think will help. Now if you want to insult me... then rate me with stars. |
This contribution was helpful to
1 thankful Users |
Follow us on